Technical FAQs

Ask a Question

The battery indicator on a Micrologic trip unit shows nothing, but the LED`s all light when the test button is pressed. Is the battery bad?

The battery indicator is not accurate. If you press the button and the LEDs light, the battery is good. It has a 7 - 10 year life.


CTA-ID : 2016315
Was this helpful?
What can we do to improve the information ?