Technical FAQs

Ask a Question

What is the contact rating for RE7 relays?

AC-15 N/C contact AC-15 N/O contact DC-13 N/O contact
3A for 24Vac 5A for 24Vac 2A for 24V
3A for 115V 5A for 115V .02 A for 115V
3A for 250V 5A for 250V 0.1A for 250V

5 amps continuous. NEMA and UL B300. Minimum switching is 12 volts at 10 mA.



CTA-ID : 2016736
Was this helpful?
What can we do to improve the information ?