Technical FAQs

Ask a Question

Do our Drives and softstarters, have a Modbus RTU or Modbus ASCII protocol?

The ATS48, ATV28 and ATV31 are strictly Modbus RTU.
The ATS46, ATV66, and ATV58 can use Modbus RTU or Modbus ASCII.
The ATV61 & ATV71 Modbus ports on the main control board are RTU.
The ATV61 & ATV71 Modbus cards are RTU and ASCII as well as Unitelway.
Refer to the specific manuals and user guides for the drive or soft starter in question for additional details.


CTA-ID : 2016732
Was this helpful?
What can we do to improve the information ?