Technical FAQs

Ask a Question

What is the difference between part numbers XCKP510 and XCKP510H44?

The H44 is a country code for Germany. The XCKP510H44 will have metric threads. As the new offering of limit switches becomes available, many of the components defined by the H codes will be available as options on the standard product, identified by part number. For example, metric conduit entries are identified by 1 as the final digit on a part number, while US conduit entries are defined by 3 as the final digit.

CTA-ID : 2016548
Was this helpful?
What can we do to improve the information ?