Technical FAQs

Ask a Question

What is the conductor range of the main grounding lug supplied on a PK27GTACU copper ground bar?

Issue:
Technical Data

Product Line:
PK Ground Bar - CU only

Cause:
Technical Data - Wire Range

Resolution:
The conductor range is #14 - #1 AWG CU (copper) only.


CTA-ID : 2016312
Was this helpful?
What can we do to improve the information ?