Technical FAQs

Ask a Question

Wants to order an FHL361005831. What is suffix 5831

Suffix 5831 is the addition of a 120-240 shunt trip and a special a special magnetic calibration of 15 times the handle rating for 1.5 cycles.
It is not UL approved

CTA-ID : 2016170
Was this helpful?
What can we do to improve the information ?