Technical FAQs

Ask a Question

On a 55391 test set we need part number for replacement on two fuse

For 24 V Test output : 250 V 200 mA
For Main : 250 V 630 mA
Obtain from third party; Schneider does not sell the fuses.


CTA-ID : 2016158
Was this helpful?
What can we do to improve the information ?