Technical FAQs

Ask a Question

Was split bus available with NQOD panelboards?

Issue:
Product Features

Product Line:
Panelboards.

Environment:
UL 67, UL 50, CSA C22.2 No.'s 20-M1989 & 94-M91, NEMA PB1, NFPA 70 Art. 408, Federal Specification W-P-115C Type 1 Class 1 , 2003 IBC, NFPA 5000, ASCE/SE17

Cause:
Splt bus is most commonly used for separating within a panelboard either lighting loads or alternatively normal/emergency power loads from other loads.  There are other applications.

Resolution:
NQOD panelboards are obsolete, superseded by NQ panelboards.  Split bus was an available feature with NQOD panelboards, as it is with NQ.



Revised 3/12/04



CTA-ID : 2016534
Was this helpful?
What can we do to improve the information ?