Technical FAQs

Ask a Question

What size pullbox is needed with 9001BF control stations?<br />

Use the standard 2.0 inch or 2.13 inch deep wall boxes. Use single gang for types BF1 and BF2 and two gang for type BF3.

CTA-ID : 2015765
Was this helpful?
What can we do to improve the information ?