Technical FAQs

Ask a Question

Why does the medium voltage metal enclosed product selector on HVL/cc add a second section when VTs are selected?<br /> <br /><br />

Because of the compact HVL/cc design, there is no physical room for them inside the switch section. The VTs must be placed in a second section and an HVL/cc switch can be provided as a disconnect switch for them. New options allow the choice of with or without an HVL/cc as a disconnect. Also, VT`s can now be mounted in the unfused sections of duplex arrangements and in incoming line terminal sections.




CTA-ID : 2015762
Was this helpful?
What can we do to improve the information ?