Technical FAQs

Ask a Question

When we order a KA or KH breaker without lugs (terminal pads only), does it come with screws for connecting busbars or ring tongue terminal lugs?<br />If do not includes such screws what suffix is necessary to add to get them included?

We do not supply terminal screws with the busbar connected KA or KH breakers. The F and K frame takes a 1/4x20 screw, customer-supplied. Screws do come with compression (ring-tongue) lugs.

CTA-ID : 2025222
Was this helpful?
What can we do to improve the information ?