Technical FAQs

Ask a Question

When we order an FA breaker without lugs (terminal pads only), does it come with screws for connecting busbars or ring tongue terminal lugs?.<br />If do not includes such screws what suffix is necessary to add to get them included?

We do not supply terminal screws with the busbar connected FA FH or FC breakers. The F frames take a 1/4x20 screw, customer-supplied. They are supplied with compression lugs.

CTA-ID : 2025221
Was this helpful?
What can we do to improve the information ?