Technical FAQs

Ask a Question

What should be filled in for the Utility Requirements in the medium voltage metal enclosed product selector?<br />

Utility requirements are either Other or EUSERC (West Coast). For other countries using this selector EUSERC is a set of standard for the Ulitities on the West Coast of the United States. Enter the name of the Utility in next field down if not EUSERC. The Utility requirements may apply to the Meter Section only or to the entire lineup if the Utility dictates that.

CTA-ID : 2015754
Was this helpful?
What can we do to improve the information ?