Technical FAQs

Ask a Question

What are the UNKNOWN defaults if UNKNOWN is chosen in a selection in the medium voltage metal enclosed product selector?<br /><br />TRY TO AVOID PICKING UNKNOWN IF POSSIBLE.<br />

UNKNOWN LUG QUANTITY - 2 PER PHASE (LINE & LOAD)

UNKNOWN LUG SIZE - 2/0 AWG TO 250 KCMIL (LINE & LOAD)
UNKNOWN MAXIMUM AVAILABLE FAULT CURRENT - 25KA SYM

UNKNOWN SYSTEM GROUNDING - 3 WIRE DELTA UNGROUNDED

NOTE: THESE UNKNOWN ANSWERS MAY ALTER THE FINAL PRICING, LAYOUT AND DIMENSIONS.




CTA-ID : 2015752
Was this helpful?
What can we do to improve the information ?