Technical FAQs

Ask a Question

Why is Visi/Vac locked out as a choice for Device Type and Rating in the medium voltage metal enclosed product selector?<br /><br />

UL may be selected for Third Party Approval on the Application Screen or your Maximum Available Fault Current is greater than 12.5 kA SYM or you have not selected a voltage for the Charging Motor/Close Voltage and the Open (Trip) Circuit Voltage.




CTA-ID : 2015747
Was this helpful?
What can we do to improve the information ?