Technical FAQs

Ask a Question

What is the horsepower rating of a H365R safety switch?

Issue:
Application

Product Line:
HD Safety Switch

Cause:
Application

Resolution:
This switch is rated for 100HP @ 480Vac, 3-phase, (using Fast acting One Time Fuses), or 250 HP @ 480Vac, 3-phase (using Dual Element Time Delay Fuses) and 125 HP @ 600Vac, 3-phase.(using Fast acting One Time Fuses), or 350 HP @ 600Vac, 3-phase (using Dual Element Time Delay Fuses) Also, 50HP @250V dc and 50hp @600V dc.
The HP ratings applicable for a safety switch are printed on the Wiring Diagram, located inside the front cover of the switch.




CTA-ID : 2015441
Was this helpful?
What can we do to improve the information ?