Technical FAQs

Ask a Question

What should be remembered about connections to Existing Equipment in the medium voltage metal enclosed product selector?<br /> <br />

Supply as much information as possible and remember that Field Service will probably have to be involved. Don`t forget to price charges for Field Service. These connections will probably require special layouts that are not available at the quotation stage of a possible order. Engineering time will have to be estimated and priced accordingly.



CTA-ID : 2015745
Was this helpful?
What can we do to improve the information ?