Technical FAQs

Ask a Question

Why isn`t there a selection for a 1200A bus connection to a transformer in the medium voltage metal enclosed product selector?<br />

There is no selection because there is no standard for it. This connection will have to be TAGGED IN. There will be an additional 22`` transition section required for indoor 1200A bus from HVL to a transformer. Contact PSEC or TAG in Smyrna Plant.

CTA-ID : 2015743
Was this helpful?
What can we do to improve the information ?