Technical FAQs

Ask a Question

What is Transformer Connection Type referring to in the medium voltage metal enclosed product selector?<br />

This applies to the type of connection (bus or cable) to the transformer, as well as if the switchgear is on the Primary or Secondary side of the transformer.




CTA-ID : 2015741
Was this helpful?
What can we do to improve the information ?