Technical FAQs

Ask a Question

Can bar type current transformers CT`s be mounted on the load side of an unfused HVL switch or Visi/Vac circuit interrupter where the fuses would normally be mounted? Can this be selected in the medium voltage metal enclosed product selector?

Yes, they can be mounted where the fuses would normally mount. At this time, this option is not available in the product selector.

CTA-ID : 2015740
Was this helpful?
What can we do to improve the information ?