Technical FAQs

Ask a Question

I have a duplex main HVL connecting to a Power-Dry transformer which will not configure or states that no Match is Found. What should I change in the medium voltage metal enclosed product selector?<br />

If you have Surge/Lightning Arresters, be sure that they are connected on the Lineside of the mains and not the loadside.



CTA-ID : 2015739
Was this helpful?
What can we do to improve the information ?