Technical FAQs

Ask a Question

What is the drive Enclosure rating for the ATV58 unit?

ATV58HU09M2 to U90N4:  IP20/open type controllers according to Standard EN50178.
ATV58HU09M2 to D46M2, ATV58HD12N4 to D79N4: Type 1 with conduit connection kit.
ATV58HC10N4X to C33N4X: IP20 on all surfaces except the bottom. IP00 on the bottom due to the power connections.

CTA-ID : 2015327
Was this helpful?
What can we do to improve the information ?