Technical FAQs

Ask a Question

How can the ATV58 drive be switched into local control if there is Serial Communication control?

The drive has a Force to Local feature.
In the I-O menu (menu 5), a logic input can be set to FLO.
This input forces the drive from serial link command to local command when the logic input is closed (state 1).
A lack of forced local does not force the drive into serial command. Serial command mode becomes active if command registers are written to.
Local command includes keypad command or terminal strip command depending on the setting of the LCC parameter in the 4 Control menu.


CTA-ID : 2015288
Was this helpful?
What can we do to improve the information ?