Technical FAQs

Ask a Question

Can the PCMCIA memory card (VW3A66901T) be used in the option extension card slot?

No.

The card should be installed in the card slot on the main control board.

If there is an option board installed on the drive, there will be two PCMCIA slots. The one in the back is on the main control board. It is the one that should be used for the memory card.


CTA-ID : 2015556
Was this helpful?
What can we do to improve the information ?