Technical FAQs

Ask a Question

How do I enter a lineup in the medium voltage metal enclosed product selector that has both HVL and HVL/cc switches?

The HVL switches must be split out from the HVL/cc switches. They cannot be entered on the same line item.
On the HVL switch that connects to the HVL/cc switches choose the lineside or loadside connection as ``connect to existing switchgear`` and enter the same Q2C number as the existing factory order number.

Do the same thing for the HVL/cc lineup on the separate line item.


CTA-ID : 2015712
Was this helpful?
What can we do to improve the information ?