Technical FAQs

Ask a Question

Do the protected LEDs with the 24-120V range such as the ZBVBG4 have the same brightness as the single voltage LED`s such as the ZBVB4 24V unit?

Yes. Past the initiating voltage of 24V, the brightness is the same no matter how much higher the input voltage is.


CTA-ID : 2015711
Was this helpful?
What can we do to improve the information ?