Technical FAQs

Ask a Question

What is the Maximum Voltage for HVL in the medium voltage metal enclosed product selector? How do I price HVL above 17.0kV?<br />

The maximum voltage for HVL is 17.0kV. HVL/cc is available up to 34.5kV. HVL switches above 17.0kV must be priced manually from the pricing guide or priced by the Project Support and Engineering Center (PSEC), 615-844-8604..




CTA-ID : 2015709
Was this helpful?
What can we do to improve the information ?