Technical FAQs

Ask a Question

What if the System Grounding is not listed in the drop down menu in the medium voltage metal enclosed product selector?<br />

Select one of the available grounding configurations and make a note in Special Pricing at no charge as to the customers actual grounding. Also, provide this information in Notes to Engineering. Only the most common grounding schemes are listed. UNKNOWN defaults to 3 Wire Delta Ungrounded. System grounding affects components such as Surge Arresters and Voltage Transformers.

CTA-ID : 2015706
Was this helpful?
What can we do to improve the information ?