Technical FAQs

Ask a Question

Do all the contacts work together on a CA2KN22G7 ? If one set welds will it prevent the others from opening?

The contacts in the CA2KN22G7 work together and if one set welds it will prevent the others from opening.

CTA-ID : 2015704
Was this helpful?
What can we do to improve the information ?