Technical FAQs

Ask a Question

What if the System Voltage for a quote or order is not listed in the drop down menu in the medium voltage metal enclosed product selector?<br />

Select the closest voltage available and make a note in Special Pricing at no charge as to the customers actual voltage. Also, provide this information in Notes to Engineering.

CTA-ID : 2015701
Was this helpful?
What can we do to improve the information ?