Technical FAQs

Ask a Question

Are the analog inputs and output isolated on the ATV58?

All the control inputs and outputs are galvanically isolated from the input power and ground but there is no isolation between the analog inputs and analog outputs.
Same applies to the J09, 0-10V converter option on Econoflex.

CTA-ID : 2015699
Was this helpful?
What can we do to improve the information ?