Technical FAQs

Ask a Question

PBQ3660G-GSL What is the GSL mean?

A= copper compression lugs
C = copper mechanical lugs (specify size)
GG = copper ground conductor
GS = gasketing on door & throat
L = special lugs (undefined)
M = automotive drip resistant
R = Class R fuse rejection clips installed


CTA-ID : 2016132
Was this helpful?
What can we do to improve the information ?