Technical FAQs

Ask a Question

Can unfused mains with bottom incoming cables be moved up from the standard Application B (inverted) position to the Application A (upper position)? This will provide increased cable termination distance of 46``.

5/15kV HVL/cc SwitchgearYes, unfused mains with bottom incoming cables can be moved up from the standard Application B (inverted) position to the Application A (upper position). This will provide increased cable termination distance of 46``.

CAUTION must be taken and a label must be provided on the bottom panel that the incoming lines are energized even though the switch is open.


CTA-ID : 2011928
Was this helpful?
What can we do to improve the information ?