Technical FAQs

Ask a Question

What do the `( )` mean at the end of catalog number PTQ4680G( )?

Need to add a suffix `V` if the plug-in unit is to be installed on vertically mounted busway or `H` if the busway is installed horizontally.


CTA-ID : 2015952
Was this helpful?
What can we do to improve the information ?