Technical FAQs

Ask a Question

What would cause inverted HVL switches to be locked out in the medium voltage metal enclosed product selector?<br /> <br />

Boric acid fuses may be selected. Boric acid fuses cannot be used with inverted switches. It is not desirable for the exhaust material from the boric acid fuses to fall down on the switch.

CTA-ID : 2015694
Was this helpful?
What can we do to improve the information ?