Technical FAQs

Ask a Question

What does the option for Switch Orientation mean in the medium voltage metal enclosed product selector?<br />

You can choose an Upright or an Inverted HVL switch, but the Selector will automatically determine the HVL/cc switch orientation based on the incoming and outgoing cables. Note: With the HVL/cc switchgear the switch blocks the entire area from front to back. (A,B,C front to back). If cables enter in one direction, they cannot exit in the same direction. Try to keep the top exiting cables together and all of the bottom exiting cables together. This will minimize the number of bus transition sections.



CTA-ID : 2015692
Was this helpful?
What can we do to improve the information ?