Technical FAQs

Ask a Question

Do we have a replacement for a XL8-AB12P112?

No, this was a Telemechanique float switch. It is obsolete. The 9035DR is NEMA 7/9 and is very similar in operation when equipped with the chain operator, 9049DCA1.

CTA-ID : 2015688
Was this helpful?
What can we do to improve the information ?