Technical FAQs

Ask a Question

Why can`t I choose cables out of a 48`` wide Meter Section in the medium voltage metal enclosed product selector?<br />

There is no standard 48`` wide meter section with provisions for outgoing cables. However, there is a standard for the 38`` wide meter section. Change the width to 38`` and them put in Special Pricing that it is to be 48`` wide. Also put this information in Notes to Engineering.




CTA-ID : 2015425
Was this helpful?
What can we do to improve the information ?