Technical FAQs

Ask a Question

What if I have a Cold Sequence Meter Section between the main switch and a transformer and need to enter it in the medium voltage metal enclosed product selector?<br />.<br />

There is no standard for this configuration. Add a 22`` empty section next to the meter section and TAG in the transformer connection charge from SW-7. Tell the selector that cables are exiting from the meter section. If the job is outdoor N3R, be sure that the outdoor enclosure charge has been included in the detailed pricing.

CTA-ID : 2015423
Was this helpful?
What can we do to improve the information ?