Technical FAQs

Ask a Question

In the Medium Voltage Metal Encl;osed Product Selector, I selected main bus for the loadside connection to a Cold Sequence Meter Section on the right. Why do I get an error message?<br />

You must answer the loadside connection as Cold Sequence Meter Section and NOT main bus. This would be true for connecting on the lineside to Hot Sequence Meter Section, or Lineside / Loadside for an Incoming / Outgoing Section

CTA-ID : 2015422
Was this helpful?
What can we do to improve the information ?