Technical FAQs

Ask a Question

Does Square D offer a Main Lug that will accept parallel(two wires) for a QO13040L200G load center?

Issue;
Product Design Features

Product Line:
QO load centers

Environment:
Main Lugs

Cause:
Application

Resolution:
NO. the main lugs ONLY accept (1) #6 - 250kcmil Al/Cu wire per phase and neutral


CTA-ID : 2015931
Was this helpful?
What can we do to improve the information ?