Technical FAQs

Ask a Question

What are the available current ratings of the HVL and HVL/cc switches with the SEM Mechanism?<br /><br />

The HVL switch is 600A only. The HVL/cc switch is 600A and 1200A.



CTA-ID : 2015411
Was this helpful?
What can we do to improve the information ?