Technical FAQs

Ask a Question

When is the SEM mechanism required on HVL and HVL/cc?<br />

The SEM mechanism is required for FUESLOGIC fuse tripping or any time when fast operation with a relay is required.



CTA-ID : 2015410
Was this helpful?
What can we do to improve the information ?