Technical FAQs

Ask a Question

How many SK5669 kits are needed for a 3 pole breaker?

Revised 05/16/05: CORRECTION --The SK5669 connector kit contains three A & C phase connectors and one B phase connector and is for use only on NQO style panelboards. This kit is used to mount both Q1 and QO circuit breakers and is not required for circuit breaker replacement purposes.


CTA-ID : 2015407
Was this helpful?
What can we do to improve the information ?