Technical FAQs

Ask a Question

Can ATV58 parameters be monitored over Ethernet without using Forced local input?

Yes. Turn off the I/O scanning using the ATV58 web page. Also, do not write to any of the command registers.
This will allow monitoring without causing the Ethernet card to take control of the drive away from the I-O terminals or the keypad.


CTA-ID : 2015919
Was this helpful?
What can we do to improve the information ?