Technical FAQs

Ask a Question

Is form B2 standard on a 9012GDW5G18 or must the form be added?

Form B2 is standard on 9012GAW21 9012GAWM21 9012GDW21 9012GDWM21 9012GGW21 & 9012GKW1 only. This provides clearance for the flange, which is larger on the low pressure devices. Form B is available on all other GAW Thru GMW, GAWM thru FWM


CTA-ID : 2015674
Was this helpful?
What can we do to improve the information ?