Technical FAQs

Ask a Question

What is Wattage Dissipated by the ATV58HD33N4 at rated load?

491 Watts for CT rated load
524 Watts for CT low noise rated load
713 Watts for VT rated load
584 Watts for VT low noise rated load


CTA-ID : 2015664
Was this helpful?
What can we do to improve the information ?