Technical FAQs

Ask a Question

What is the edgewise hanger used for the 100 amp version of PowerBus225?

The only hanger available for the 100 amp version of Powerbus 225 is a PB100FH. It will mount the bus edgewise so that the plug-in units will mount on the sides of the busway.


CTA-ID : 2015530
Was this helpful?
What can we do to improve the information ?