Technical FAQs

Ask a Question

Can a DTU323 double throw switch be used for the application to switch one power source between two loads?

Yes, as is the case for all F series 30 - 100A double throw switches.


CTA-ID : 2015535
Was this helpful?
What can we do to improve the information ?