Technical FAQs

Ask a Question

What will the coils on a 8501 type K relay operate at?

The will operate at AC: +10, -15% of Nominal Voltage at 25 deg C (77 deg F)
They will operate at DC: +10, -25% of Nominal Voltage at 25 deg C (77 deg F)





CTA-ID : 2015399
Was this helpful?
What can we do to improve the information ?